:MEASure:EYE:PAM:PMIN:STATus:REASon?

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Query Syntax

:MEASure:EYE:PAM:PMIN:STATus:REASon?

Query Response

Refer to the table "Possible Common :STATus:REASon? Query Responses".

Description

Returns a string that explains the reason for a failed :MEASure:EYE:PAM:PMIN measurement. If the measurement was successful, a null string is returned. Use the :MEASure:EYE:PAM:PMIN:STATus? query to determine if the measurement has failed. Additional information about the failure may be available using the :MEASure:EYE:PAM:PMIN:STATus:DETails? query.

Requires FlexDCA revision A.07.60 and above.