:MEASure:EYE:PAM:SKEW:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:SKEW:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | CGMemory{1:8} | FUNCtion{1:16}}
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:MEASure:EYE:PAM:SKEW:SOURce?
Description
Selects the source waveform on which to perform the SKEW measurement for PAM4 or NRZ signals. The source must be an eye diagram.
Requires FlexDCA revision A.04.50 and above.