:MEASure:EYE:PNMargin:EYE

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4

Command Syntax

:MEASure:EYE:PNMargin:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:EYE:PNMargin:EYE?

Query Response

 {EYE0 | EYE1 | EYE2}

Description

This command allows you to select an eye on PAM4 signal for a Partial Noise Margin measurement (:MEASure:EYE:PNMARgin) measurement. The default setting is EYE0.

PAM4 Waveform

Requires FlexDCA revision A.05.70 and above.