:MEASure:EYE:PNMargin:SIDe

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4

Command Syntax

:MEASure:EYE:PNMargin:SIDe {LEFT | RIGHt}

Query Syntax

:MEASure:EYE:PNMargin:SIDe?

Query Response

 {LEFT | RIGH}

Description

Selects the side of the waveform on which to perform the Partial Noise Margin measurement (:MEASure:EYE:PNMARgin). The default setting is LEFT.

Requires FlexDCA revision A.05.70 and above.