:MEASure:EYE:PSER:SIDe

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PSER:SIDe {LEFT | RIGHt}

Query Syntax

:MEASure:EYE:PSER:SIDe?

Query Response

 {LEFT | RIGH}

Description

Selects the side of the waveform on which to perform a Partial SER measurement (:MEASure:EYE:PSER). The default setting is LEFT.

Requires FlexDCA revision A.05.70 and above.