:MEASure:EYE:PSER:LOCation?

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Query Syntax

:MEASure:EYE:PSER:LOCation?

Description

Returns an index for the location of Partial SER measurement (:MEASure:EYE:PSER) in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.

Requires FlexDCA revision A.05.70 and above.