:MEASure:EYE:RN:RNSValue:LEVel{0|1|2|3}

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:RN:RNSValue <random_noise>

<random_noise> is a double.

Query Syntax

:MEASure:EYE:RN:RNSValue?

Description

For a RN measurement, sets the value of RN used for RN stabilization for the selected eye level. PAM4 signals have four possible levels: 0, 1, 2, and 3. NRZ signals has two possible levels: 0 and 1. There are actually four commands, one for each eye level on the signal.

  • :MEASure:EYE:DI:RNSValue:LEVel3 (for PAM4 only)
  • :MEASure:EYE:DI:RNSValue:LEVel2 (for PAM4 only)
  • :MEASure:EYE:DI:RNSValue:LEVel1 (for NRZ and PAM4)
  • :MEASure:EYE:DI:RNSValue:LEVel0 (for NRZ and PAM4)

To measure the RN, switch the N1000A to Jitter Mode and measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. Use the :MEASure:EYE:RN:RNSTabilize command to turn on or off the use of RN stabilization.

Command Description
RNSValue:LEVel3 Applies to level 3.
RNSValue:LEVel2 Applies to level 2.
RNSValue:LEVel1 Applies to level 1.
RNSValue:LEVel0 Applies to level 0.

Linked RN Stabilization (On / Off) Commands

The following commands are equivalent. Turn on setting on and they are all turned on.

Linked RN Value Commands

The RNSValue:LEVel commands for the same eye level are equivalent. Use one of a commands to enter a value for one level on a measurement and it is changed for the other three measurements. For example, enter the level two value for a DI measurement and the level two value is also entered for RN and TI measurements.

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.05.30 and above.