:MEASure:EYE:TJ:LOCation?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Query Syntax
:MEASure:EYE:TJ:LOCation?
Description
Returns an index for the location of the TJ measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.
Requires Option 401, Advanced Eye Analysis Software license.
Requires FlexDCA revision A.02.50 and above.