:MEASure:JITTer:DDJSymbol:EARLiest?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Query Syntax

:MEASure:JITTer:DDJSymbol:EARLiest?

Description

Returns a string of two comma-separated values for the earliest measured edge in the DDJ vs. symbol graph. The string includes the symbol number followed by the DDJ value, for example "70,-8.579983e-014". The DDJ value has units of time or unit interval as specified by the :MEASure:JITTer:DEFine:UNITs command.

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :MEASure:JITTer:DDJVsbit:EARLiest.

Example Command Sequence

:SYSTem:MODE JITTer
:MEASure:JITTer:DDJSymbol:EARLiest?