:MEASure:JITTer:DDJSymbol:LATest?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Query Syntax

:MEASure:JITTer:DDJSymbol:LATest?

Description

Returns a string of two comma-separated values for the latest measured edge in the DDJ vs. symbol graph. The string includes the symbol number followed by the DDJ value for example "108,7.927662e-014". The DDJ value has units of time or unit interval as specified by the :MEASure:JITTer:DEFine:UNITs command.

Requires FlexDCA revision A.05.60 and above.

This command replaces deprecated command :MEASure:JITTer:DDJVsbit:LATest.

Example Command Sequence

:SYSTem:MODE JITTer
:MEASure:JITTer:DDJSymbol:EARLiest?