:MEASure:JITTer:DDJVsbit:EARLiest?
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:JITTer:DDJSymbol:EARLiest command instead.
Query Syntax
:MEASure:JITTer:DDJVsbit:EARLiest?
Description
Returns a string of two comma-separated values for the earliest measured edge in the DDJ vs. bit graph. The string includes the bit number followed by the DDJ value, for example "70,-8.579983e-014". The DDJ value has units of time or unit interval as specified by the :MEASure:JITTer:DEFine:UNITs command.
Requires Jitter Mode license.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:JITTer:DDJVsbit:EARLiest?