:MEASure:JITTer:DDJVsbit:LATest?
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:JITTer:DDJSymbol:LATest command instead.
Query Syntax
:MEASure:JITTer:DDJVsbit:LATest?
Description
Returns a string of two comma-separated values for the latest measured edge in the DDJ vs. bit graph. The string includes the bit number followed by the DDJ value for example "108,7.927662e-014". The DDJ value has units of time or unit interval as specified by the :MEASure:JITTer:DEFine:UNITs command.
Requires Jitter Mode license.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:JITTer:DDJVsbit:EARLiest?