:MEASure:JITTer:LIST:MOVe
Command Syntax
:MEASure:JITTer:LIST:MOVe <source index>, <destination index>
<index> is an int.
Query Syntax
:MEASure:JITTer:LIST:MOVe?
Description
In Jitter Mode's Jitter results table for NRZ waveforms, moves the specified measurement to another position in the table. Both the <source index> and <destination index> arguments are required. The indexes are integers that identify a measurement position in the table. The measurement list is indexed starting at 1 which is the first (top most) measurement in the list. The second measurement from the top is identified as 2, and so forth.
To get the index value for a listed measurement, use the measurement's :LOCation? child command. For example, use for a Duty Cycle Distortion (DCD) measurement, you would send :MEASure:JITTer:DCD:LOCation? to return the index. Use this index as the <source index> for the move. In your program, you do not need to first select the measurement before you send this command to move the measurement.
The Jitter panel lists all of Jitter Mode's default standard time measurements. The following additional time measurements can be added to this panel with these commands:
- JN total (
:MEAS:JITTer:JN) - Data Dependent Pulse Width Shrinkage (DDPWS) (
:MEAS:JITTer:DDPWs) - Uncorrelated Jitter (UJ) (
:MEAS:JITTer:UJ) - F/2 jitter (J(F/2))
:MEAS:JITTer:FOVer2
To move measurements shown in Jitter Mode's Amplitude panel, use the :MEASure:AMPLitude:LIST:MOVe command.
Example Command Sequence
This script assumes that Jitter Mode's Jitter table is displayed with the DCD measurement listed. The script returns the measurement's index location. Then the measurement is moved to the top of the table (index 1).
Moving a Measurement Result
import pyvisa as visa # import VISA library
rm = visa.ResourceManager()
FlexDCA = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR')
FlexDCA.timeout = 5000 # Set connection timeout to 5s
FlexDCA.read_termination = '\n'
FlexDCA.write_termination = '\n'
index = FlexDCA.query(':MEASure:JITTer:DCD:LOCation?')
print('DCD index: ' + index)
FlexDCA.write('MEAS:JITTer:LIST:MOVe ' + index +', 1')
index = FlexDCA.query(':MEASure:JITTer:DCD:LOCation?')
print('New DCD index: ' + index)
FlexDCA.write(':SYSTem:GTLocal')
FlexDCA.close()