:MEASure:AMPLitude:LIST:MOVe
Command Syntax
:MEASure:AMPLitude:LIST:MOVe <source index>, <destination index>
<index> is an int.
Query Syntax
:MEASure:AMPLitude:LIST:MOVe?
Description
In Jitter Mode's Amplitude results table for NRZ waveforms, moves the specified measurement to another position in the table. Both the <source index> and <destination index> arguments are required. The indexes are integers that identify a measurement position in the table. The measurement list is indexed starting at 1 which is the first (top most) measurement in the list. The second measurement from the top is identified as 2, and so forth.
To get the index value for a listed measurement, use the measurement's :LOCation? child command. For example, use for a Fall Time measurement, you would send :MEASure:AMPLitude:Q:LOCation? to return the index. Use this index as the <source index> for the move. In your program, you do not need to first select the measurement before you send this command to move the measurement.
The Amplitude panel lists all of Jitter Mode's default standard amplitude measurements. The following additional amplitude measurements to this panel with these commands:
- Relative Intensity Noise (RIN) (
:MEAS:AMPLitude:RINoise) - UN (Uncorrelated Noise) (
:MEAS:AMPLitude:UN) - Preshoot (PCIe) (
:MEAS:AMPLitude:PPCie) - De-emphasis (PCIe) (
:MEAS:AMPLitude:DEPCie)
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
To move measurements shown in Jitter Mode's Jitter panel, use the :MEASure:JITTer:LIST:MOVe command.
Example Command Sequence
This script assumes that Jitter Mode's Amplitude table is displayed with the RN Ones and RN Zeros measurements listed. The script specifies the RN Ones and then returns the measurements index location. Then the measurement is moved to the top of the table (index 1).
Moving a Measurement Result
import pyvisa as visa # import VISA library
rm = visa.ResourceManager()
FlexDCA = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR')
FlexDCA.timeout = 5000 # Set connection timeout to 5s
FlexDCA.read_termination = '\n'
FlexDCA.write_termination = '\n'
FlexDCA.write(':MEASure:AMPLitude:RN:LEVel LEVel1') # select RN Ones
index = FlexDCA.query(':MEASure:AMPLitude:RN:LOCation?')
print('RN Ones index: ' + index)
FlexDCA.write('MEAS:AMPLitude:LIST:MOVe ' + index +', 1')
index = FlexDCA.query(':MEASure:AMPLitude:RN:LOCation?')
print('New RN index: ' + index)
FlexDCA.write(':SYSTem:GTLocal')
FlexDCA.close()