:MEASure:JITTer:OJITter:EOJ:LOCation?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter
Query Syntax
:MEASure:JITTer:OJITter:EOJ:LOCation?
Query Results
"<row location>"
For example, "27".
Description
Returns an index string that identifies the location of the measurement results in the Output Jitter panel. This measurement is based on a specific edge as specified by the :MEASure:JITTer:OJITter:EOJ:MEASure:JITTer:OJITter:EOJ:ECATegory command. The location index can be used to select the measurement for a measurement limit test. (:LTESt:MEASure:MLIMit:SOURce:LOCation command).
If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.05.70 and above.