:MEASure:JITTer:OJITter:EOJ:STATus:REASon?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Query Syntax

:MEASure:JITTer:OJITter:EOJ:STATus:REASon?

Query Response

Refer to the table "Possible Common :STATus:REASon? Query Responses".

Description

Returns a string that explains the reason for a failed :JITTer:OJITter:EOJ measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :STATus:DETails? sibling query. Use the :JITTer:OJITter:EOJ:STATus? parent query to determine if the measurement has failed.

Requires FlexDCA revision A.05.70 and above.

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.

For example, to return the status of the measurement, :MEASure:JITTer:OJITter:EOJ

flex.write(':MEASure:JITTer:OJITter:EOJ:SOURce CHAN1A')
if flex.query(':MEASure:JITTer:OJITter:EOJ:STATus?') == 'CORR';
    measurement = flex.query(':MEASure:JITTer:OJITter:EOJ?')
else:
	details = flex.query(':MEASure:JITTer:OJITter:EOJ:STATus:DETails?')
	reason = flex.query(':MEASure:JITTer:OJITter:EOJ:STATus:REASon?')