:MEASure:JITTer:OJITter:HISTogram:SAMPles?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter
Query Syntax
:MEASure:JITTer:OJITter:HISTogram:SAMPles?
Description
Returns the number of samples that are included in the Output Jitter Histogram data that is returned using the :MEASure:JITTer:OJITter:HISTogram? query. To turn on Jitter mode's 12-Edge Output Jitter measurements for PAM4 signals, use the :MEASure:JITTer:OJITter:STATe command.
Requires FlexDCA revision A.05.70 and above.