:MEASure:JITTer:OJITter:HISTogram:XORigin?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Query Syntax

:MEASure:JITTer:OJITter:HISTogram:XORigin?

Description

Returns the X-axis origin (time) for the Output Jitter Histogram that is returned using the :MEASure:JITTer:OJITter:HISTogram? query. To turn on Jitter mode's 12-Edge Output Jitter measurements for PAM4 signals, use the :MEASure:JITTer:OJITter:STATe command.

Requires FlexDCA revision A.05.70 and above.