:MEASure:JITTer:OJITter:JNU:DISPlay

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Command Syntax

:MEASure:JITTer:OJITter:JNU:DISPlay {ON | OFF | 1 | 0}

Query Syntax

:MEASure:JITTer:OJITter:JNU:DISPlay?

Query Response

 {ON | OFF | 1 | 0}

Description

Expands or contracts the display of the IEEE JNU measurement results in the displayed Output Jitter panel. Select ON, the default value, to expand the panel to show JNU measurement results for all edges. When OFF is selected, only the JNU result for all edges can be queried using the :MEASure:JITTer:OJITter:JNU? query.

Requires FlexDCA revision A.05.85 and above.