:MEASure:JITTer:OJITter:JNU:LOCation?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Query Syntax

:MEASure:JITTer:OJITter:JNU:LOCation?

Query Results

"<row location>"

For example, "1".

Description

Returns an index string that identifies the location of the :MEASure:JITTer:OJITter:JNU measurement results in the Output Jitter panel. This measurement is based on a specific edge as specified by the :MEASure:JITTer:OJITter:JNU:ECATegory command. The locaton index can be used to select the measurement for a measurement limit test. (:LTESt:MEASure:MLIMit:SOURce:LOCation command).

If the measurement is not listed in the table, a "−1" is returned.

Requires FlexDCA revision A.05.85 and above.