:MEASure:MARKer:DX:STATus:REASon?
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:MARKer:DX:STATus:REASon?
Query Response
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
Returns a string that explains the reason for a failed XDELta measurement. If the measurement was successful, a null string is returned. Use the STATus? query to determine if the measurement has failed.
Requires FlexDCA revision A.03.00 and above.