:MEASure:MARKer:XDELta:STATus?

Command:
Deprecated

Deprecated command. For FlexDCA revision A.03.00 and above.

Query Syntax

:MEASure:MARKer:XDELta:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the XDELta measurement. Use the STATus:REASon? child query to determine the reason for a invalid or questionable measurement.