:MEASure:MTESt:MHRegion:LOCation?
Meas. mode:
                                                Eye
                                            Flex Apps:
                                            Query Syntax
:MEASure:MTESt{N}:MHRegion{1:16}:LOCation?
                                            {N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2: selects mask 2.
Description
Returns an index for the location of the MHRegion measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.