:MEASure:MTESt:MHRegion:STATus:REASon?
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
FlexRT
FlexRT
FlexRT
Query Syntax
:MEASure:MTESt{N}:MHRegion{1:16}:STATus:REASon?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2: selects mask 2.
Query Response
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
Returns a string that explains the reason for a failed :MTESt:MHRegion measurement. If the measurement was successful, a null string is returned.
Additional information about the failure may be available using the :STATus:DETails? sibling query. Use the :MTESt:MHRegion:STATus? parent query to determine if the measurement has failed.