:MEASure:OSCilloscope:LIST:REMove
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:LIST:REMove <index>
<index> is an int.
Description
Removes the selected measurement from the active measurement list, which is displayed in the Results table. The argument is an index number that specifies the measurement to be removed. The active measurement list is indexed starting at 1. As a result, the first (top most) measurement in the list is identified as 1, the second measurement from the top is identified as 2, and so forth. To get the index value for a specific measurement, use the :LOCation? child command for the targeted measurement. For example, use :MEASure:OSCilloscope:FALLtime:LOCation?.
Example Command Sequence
Read the location of the falltime result in the table, send the REMove command with the returned value. In this case 2.
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:FALLtime:LOCation? … … :MEASure:OSCilloscope:LIST:REMove 2