:MEASure:OSCilloscope:PAM:LINearity:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
PAM4
Command Syntax
:MEASure:OSCilloscope:PAM:LINearity:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | FUNCtion{1:16} | WMEMory{1:8}}
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:MEASure:OSCilloscope:PAM:LINearity:SOURce?
Description
Selects the source waveform on which to perform the PAM:LINearity measurement for PAM4 or NRZ signals. The source must be a displayed single-valued waveform.
Requires FlexDCA revision A.04.50 and above.