:MEASure:OSCilloscope:PAM:RMS:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4

Command Syntax

:MEASure:OSCilloscope:PAM:RMS:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | FUNCtion{1:16} | WMEMory{1:8}}

{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.

Query Syntax

:MEASure:OSCilloscope:PAM:RMS:SOURce?

Description

Selects the source waveform on which to perform the :RMS measurement for PAM4 or NRZ signals. The source must be a displayed single-valued waveform.

Requires FlexDCA revision A.04.50 and above.