:MEASure:OSCilloscope:TEDGe:DIRection

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:OSCilloscope:TEDGe:DIRection  {RISing | FALLing}

Query Syntax

:MEASure:OSCilloscope:TEDGe:DIRection?

Description

For the Time-at-Edge measurement, specifies the edge direction used to identify the waveform's edge: rising or falling. To specify the edge number, use the :OSCilloscope:TEDGe:NUMBer command. To specify the edge threshold, use the :OSCilloscope:TEDGe:THReshold command.

Example Command Sequence

:SYSTem:MODE OSCilloscope
:MEASure:OSCilloscope:TEDGe:SOURce CHAN2B
:MEASure:OSCilloscope:TEDGe:DIRection RISing
:MEASure:OSCilloscope:TEDGe:NUMBer 2
:MEASure:OSCilloscope:TEDGe:THReshold MIDDle
:MEASure:OSCilloscope:TEDGe
:MEASure:OSCilloscope:TEDGe?