:MEASure:OSCilloscope:TEDGe:THReshold
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:TEDGe:THReshold {UPPer | MIDDle | LOWer}
Query Syntax
:MEASure:OSCilloscope:TEDGe:THReshold?
Description
For the Time-at-Edge measurement, specifies the edge threshold used to identify the waveform's edge: upper, middle, or lower. To specify the edge number, use the :OSCilloscope:TEDGe:NUMBer command. To specify the edge direction, use the :OSCilloscope:TEDGe:DIRection command.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:TEDGe:SOURce CHAN2B :MEASure:OSCilloscope:TEDGe:DIRection RISing :MEASure:OSCilloscope:TEDGe:NUMBer 2 :MEASure:OSCilloscope:TEDGe:THReshold MIDDle :MEASure:OSCilloscope:TEDGe :MEASure:OSCilloscope:TEDGe?