:MEASure:OSCilloscope:TEDGe:NUMBer
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:TEDGe:NUMBer <edge_number>
<edge_number> is an int.
Query Syntax
:MEASure:OSCilloscope:TEDGe:NUMBer?
Description
For the Time-at-Edge measurement, specifies the edge number used to identify the waveform's edge. To specify the edge threshold, use the :OSCilloscope:TEDGe:THReshold command. To specify the edge direction, use the :OSCilloscope:TEDGe:DIRection command.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:TEDGe:SOURce CHAN2B :MEASure:OSCilloscope:TEDGe:DIRection RISing :MEASure:OSCilloscope:TEDGe:NUMBer 2 :MEASure:OSCilloscope:TEDGe:THReshold MIDDle :MEASure:OSCilloscope:TEDGe :MEASure:OSCilloscope:TEDGe?