:MEASure:TDR:DELTatime:EDIRection
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:DELTatime:EDIRection{1:2} {RISing | FALLing | EITHer}
Query Syntax
:MEASure:TDR:DELTatime:EDIRection?
Description
For the Delta Time measurement, specifies the waveform's edge direction used to identify the first or second measurement edge: rising, falling or either. To set the edge number, use the :TDR:DELTatime:ENUMber command. To set the edge threshold, use the :TDR:DELTatime:ETHReshold command.
Requires FlexDCA revision A.04.00 and above.