:MEASure:TDR:DELTatime:ENUMber
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:DELTatime:ENUMber{1:2} <edge_number>
<edge_number> is an int.
Query Syntax
:MEASure:TDR:DELTatime:ENUMber?
Description
For the Delta Time measurement, specifies the waveform's edge number to be used to identify the first or second measurement edge. To set the edge direction, use the :TDR:DELTatime:EDIRection command. To set the edge threshold, use the :TDR:DELTatime:ETHReshold command.
Requires FlexDCA revision A.04.00 and above.