:MEASure:TDR:DELTatime:ETHReshold
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:DELTatime:ETHReshold{1:2} {UPPer | MIDDle | LOWer}
Query Syntax
:MEASure:TDR:DELTatime:ETHReshold?
Description
For the Delta Time measurement, specifies the waveform's edge threshold to be used to identify the first or second measurement edge. To set the edge direction, use the :TDR:DELTatime:EDIRection command. To set the edge number, use the :TDR:DELTatime:ENUMber command.
Requires FlexDCA revision A.04.00 and above.