:MEASure:TDR:TVOLt:EDIRection
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:TVOLt:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:TDR:TVOLt:EDIRection?
Description
For the Time-at-Amplitude measurement, specifies the edge direction used to identify the waveform location at which to perform the measurement. The edge can be identified as rising or falling. To specify the edge number, use the :TDR:TVOLt:ENUMber command. To specify the amplitude value, use the :TDR:TVOLt:YVALue command.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:SYSTem:MODE TDR :MEASure:TDR:TVOLt:SOURce TRACe8 :MEASure:TDR:TVOLt:EDIRection RISing :MEASure:TDR:TVOLt:ENUMber 1 :MEASure:TDR:TVOLt:YVALue 100E-03 :MEASure:TDR:TVOLt :MEASure:TDR:TVOLt?