:MEASure:TDR:TVOLt:YVALue
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:TVOLt:YVALue <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:TDR:TVOLt:YVALue?
Description
For the Time-at-Amplitude measurement, specifies the amplitude value at which to perform the measurement. To specify the edge direction, use the :TDR:TVOLt:EDIRection command. To specify the edge number, use the :TDR:TVOLt:ENUMber command.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:SYSTem:MODE TDR :MEASure:TDR:TVOLt:SOURce TRACe2 :MEASure:TDR:TVOLt:EDIRection RISing :MEASure:TDR:TVOLt:ENUMber 1 :MEASure:TDR:TVOLt:YVALue 100E-03 :MEASure:TDR:TVOLt :MEASure:TDR:TVOLt?