:RTSCope:CONNect:HOST
Instrument:
UXR Scope
Flex Apps:
FlexRT
Command Syntax
:RTSCope:CONNect:HOST "hostname"
Where "hostname" is a string that identifies the UXR-series oscilloscope's Computer Name.
Query Syntax
:RTSCope:CONNect:HOST?
Description
Sets or queries the current host name of a UXR-series oscilloscope for connecting the oscilloscope via a LAN. If FlexRT is running on the UXR-series oscilloscope, you can use localhost as the host name. Use the :RTSCope:CONNect command to make the actual connection.
Requires FlexDCA revision A.06.70 and above.
Example Command
:RTSCope:CONNect:HOST "localhost"