:RTSCope:CONNect:STATe?
Instrument:
UXR Scope
Flex Apps:
FlexRT
Query Syntax
:RTSCope:CONNect:STATe?
Query Response
{CONN | NCON | TOUT}
Description
Returns the state of the LAN connection between FlexRT and a UXR-series oscilloscope. Returns one of the following strings:
CONN- A connection is established to the oscilloscope.
NCON- A connection is not established.
TOUT- A connection to an oscilloscope has timed out.
Requires FlexDCA revision A.06.70 and above.
Example Command
:RTSCope:CONNect:STATe?