:SLOT:TRIGger:BRATe
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :SLOT:TRIGger:SRATe command.
Command Syntax
:SLOTN:TRIGger:BRATe <rate>
Where N identifies a specific module by slot and must be selected from {1:8}.
<rate> is a double.
Query Syntax
:SLOTN:TRIGger:BRATe?
Description
When using pattern lock, enters the symbol-rate of the trigger source. Automatic detection must be turned off before the entered symbol rate setting is applied (:SLOT{1:8}:TRIGger:BRATe:AUTodetect).
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command Sequence
:SLOT5:TRIGger:BRATe:AUTodetect OFF :SLOT5:TRIGger:BRATe 2.0E+10 :TRIGger:PLOCk ON