:SLOT:TRIGger:BRATe:AUTodetect
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :SLOT:TRIGger:SRATe:AUTodetect command.
Command Syntax
:SLOTN:TRIGger:BRATe:AUTodetect {ON | OFF | 1 | 0}
Where N identifies a specific module by slot and must be selected from {1:8}.
Query Syntax
:SLOTN:TRIGger:BRATe:AUTodetect?
Query Response
{1 | 0}
Description
When using pattern lock, enables or disables automatic bit-rate detection. When turned off, use the :SLOT{1:8}:TRIGger:BRATe command to set the bit rate. When turned on, send the :TRIGger:PLOCk ON or :SYSTem:PAUTodetect command to actually detect the bit rate.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Example Command Sequence
:SLOTN:TRIGger:BRATe:AUTodetect ON
:TRIGger:PLOCk ON