:SLOT:TRIGger:SRATe
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:SRATe <rate>
Where the {1:8} specifier identifies a module slot.
<rate> is a double.
Query Syntax
:SLOT{1:8}:TRIGger:SRATe?
Description
Enter the symbol-rate of the trigger source when using pattern lock. Automatic detection must be turned off before the entered symbol rate setting is applied (:SLOT:TRIGger:SRATe:AUTodetect).
This command applies to an N1092A/B/D Option-PLK DCA-M.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :SLOT:TRIGger:BRATe.
Example Command Sequence
:SLOT5:TRIGger:SRATe:AUTodetect OFF :SLOT5:TRIGger:SRATe 2.0E+10 :TRIGger:PLOCk ON