:SLOT:TRIGger:SRATe:AUTodetect
Command Syntax
:SLOT{1:8}:TRIGger:SRATe:AUTodetect {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies a module slot.
Query Syntax
:SLOT{1:8}:TRIGger:SRATe:AUTodetect?
Query Response
{1 | 0}
Description
Enables or disables automatic detection of symbol-rate for pattern lock. A default setup turns automatic detection on.
When automatic detection is turned off, use the :SLOT:TRIGger:SRATe command to enter the symbol rate. When automatic is enabled, send the :TRIGger:PLOCk ON or :SYSTem:PAUTodetect command to actually detect the symbol rate.
This command requires that the type of Clock Ratio be first set to Integer instead of Fractional. Use the :SLOT:TRIGger:DCDRatio:TYPE command to select an integer clock ratio.
This command applies to an N1092A/B/D Option-PLK DCA-M.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :SLOT:TRIGger:BRATe:AUTodetect.
Example Command Sequence
:SLOT{1:8}:TRIGger:SRATe:AUTodetect ON
:TRIGger:PLOCk ON