:SPRocess:BESSel:BANDwidth

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:BESSel:BANDwidth <cutoff_frequency>

<cutoff_frequency> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:BESSel:BANDwidth?

Description

Specifies the cutoff frequency in Hertz of a Bessel filter operator. To configure the filter's Aliased Noise Processing, use the :SPRocess:BESSel:PNOise command.

Example Command Sequence

:FUNCtion2:FOPerator BESSel
:SPRocess2:BESSel:BANDwidth 10.5E6
:SPRocess2:PNOise ON
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.