:SPRocess:BESSel:PNOise:BANDwidth:AUTo
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Command Syntax
:SPRocessN:BESSel:PNOise:BANDwidth:AUTo {OFF | ON}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:BESSel:PNOise:BANDwidth:AUTo?
Description
Turns on or off the use of automatic bandwidth setting when using noise preservation. If the setting is off, enter the desired bandwidth using the :BANDwidth parent command. To turn on noise preservation, use the :PNOise parent command.
Requires FlexDCA revision A.05.60 and above.