:SPRocess:DDEMbed

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DDEMbed {DIFFerential | CMODe | SPLus | SMINus}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DDEMbed?

Description

Selects the output type of a 4-Port DeEmbedding operator. Use the :SPRocess:DDEMbed:BANDwidth command to specify the function's bandwidth. Use the :SPRocess:DDEMbed:BLIMit command to specify a bandwidth filter. Use the :SPRocess:DDEMbed:FNAMe command to open an existing network file that models your test setup.

DIFFerential
Specifies a differential output signal.
CMODe
Specifies a common mode output signal.
SPLus
Specifies a single-ended (+) output signal.
SMINus
Specifies a single-ended (−) output signal.

Example Command Sequence

:FUNCtion2:FOPerator DDEMbed
:SPRocess2:DDEMbed:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\De-Embedding Networks\DUT_4.tf4"
:SPRocess2:DDEMbed DIFFerential
:SPRocess2:DDEMbed:BANDwidth:AUTo ON
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.