:SPRocess:DDEMbed:BANDwidth:AUTo

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DDEMbed:BANDwidth:AUTo {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DDEMbed:BANDwidth:AUTo?

Query Response

{1 | 0}

Description

Turns on or off automatic bandwidth setting for a 4-Port DeEmbedding operator.. When off, use the parent command (:SPRocess:DDEMbed:BANDwidth) to enter the bandwidth. Selects a 10 dB bandwidth that is based on the loaded S-parameter file. This is the bandwidth when the S-parameters fall by 10 dB.

Example Command Sequence

:FUNCtion2:FOPerator DDEMbed
:SPRocess2:DDEMbed:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\De-Embedding Networks\DUT_4.tf4"
:SPRocess2:DDEMbed:FMODel ON  // Flips  S-parameters ports
:SPRocess2:DDEMbed:BANDwidth:AUTo OFF
:SPRocess2:DDEMbed:BANDwidth:BLIMit GAUSsian
:SPRocess2:DDEMbed:BANDwidth 7.5E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.