:SPRocess:DEMBed:BANDwidth

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:DEMBed:BANDwidth <bandwidth>

<bandwidth> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DEMBed:BANDwidth?

Description

Specifies the bandwidth, in Hertz, of a 2-Port DeEmbedding operator. This minimizes the effects of noise. The :SPRocess:DEMBed:BANDwidth:AUTo child command must be set OFF, before you can set the bandwidth manually. Use the :SPRocess:DEMBed:BANDwidth:BLIMit command to select the type of bandwidth filter used. Use the :SPRocess:DEMBed:FNAMe command to open an existing network file that models your test setup. To configure the filter's Aliased Noise Processing, use the :SPRocess:DEMBed:PNOise command.

Example Command Sequence

:FUNCtion2:FOPerator DEMBed
:SPRocess2:DEMBed:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\De-Embedding Networks\DUT_4.tf2"
:SPRocess2:DEMBed:BANDwidth:AUTo OFF
:SPRocess2:DEMBed:BANDwidth 8.5E9
:SPRocess2:DEMBed:BLIMit GAUSsian
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.