:SPRocess:SINC:BANDwidth
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SPRocessN:SINC:BANDwidth <cutoff_frequency>
<cutoff_frequency> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocess:SINC:BANDwidth?
Description
Specifies the cutoff frrequency in Hertz of a Sin(x)/x, or sinc(x), operator (:FUNCtion:FOPerator SINC
).
Requires FlexDCA revision A.05.60 and above.