:SPRocess:SINC:PNOise:BANDwidth
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:SPRocessN:SINC:PNOise:BANDwidth <bandwidth>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:SINC:PNOise:BANDwidth?
Description
Sets the bandwidth used when preserving the input waveform's noise on the output waveform. To turn on noise preservation, use the :PNOise parent command. The :BANDwidth:AUTO child command must be set to OFF otherwise the function automatically determines the bandwidth to use.
Requires FlexDCA revision A.05.60 and above.