:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE?
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE? "<model number>"
Where <model number> is the feature/model number string that identifies a Manufacturing , Research and Development , or Signal Integrity package license.
Query Response
<year,month,day>
Description
For the specified license package model number, returns software support expiration date in the form "year,month,day". For example, "2018,7,1". This is the date that the current licenses expires. This string is located inside the package license file and is listed in the following table.
| Parameter | Example Returned Feature/Model Number String |
Description |
|---|---|---|
| L-MFG | N1010200A | Manufacturing Package |
| L-RND | N1010100A | Research and Development Package |
| L-SNT | N1010300A | Signal Integrity Package |
Requires FlexDCA revision A.05.80 and above.
Example Query
:SYSTem:LKEY:SOFTware:SUPPort:EXPiration:DATE? "N1010200A"