:SYSTem:SOFTware:FEATures:VERSion?
Query Syntax
:SYSTem:SOFTware:FEATures:VERSion? "<software feature>"
Where <software feature> is the identification string representing an enabled software feature.
Query Response
{1 | 0}
Description
Returns the version date of an enabled software feature in the form of "1.000". The specified feature must be enabled for use. Before sending this command, always confirm that the software feature is enabled using the :SYSTem:SOFTware:FEATures:ENABled? command. The following table lists the valid software feature parameters for this query. These are the same strings returned by the *OPT? common command. Notice that valid parameters start with the "F-" characters. Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message.
| Query Argument | Software Feature |
|---|---|
| F-AEYE | Advanced Eye Analysis |
| F-AFR | Automatic Fixture Removal in TDR Mode |
| F-ATDR | Enhanced Impedance and S-Parameters |
| F-AWG | Keysight Arbitrary Waveform Generator Control |
| F-EQ | Equalizers (CTLE, DFE, LFE) |
| F-FEYE | FlexEye Independent Eye Acquisition and Analysis |
| F-FLEX | FlexDCA Remote Access Software |
| F-JIT | Enhanced Jitter Analysis |
| F-PAM | PAM-N Analysis Software |
| F-PTDQ | Partial TDECQ, Noise Margin, and SER Measurements |
| F-SIM | InfiniiSim-DCA Waveform Transformation Toolset |
| F-RRX | Provides a reference receiver Waveform Signal Processing operator that allows joint FFE/DFE optimization |
| F-TDEC | NRZ TDEC Measurement |
| F-TDQ | TDECQ Measurement and Equalizer |
| F-UDI | Unrestricted Data File Import |
| F-UDMO | User Defined Measurements and Operators |
Requires FlexDCA revision A.06.00 and above.
Example Query
:SYSTem:SOFTware:FEATures:VERSion? "F-AWG"